AnsweredAssumed Answered

vrf Debug help

Question asked by VRFuser on Feb 8, 2000
When I saw this I unchecked the setting of Auto Line Routing in the
preferences of HP VEE.
Hope this helps.

Hal Cornelius
Research Planning Inc.
China Lake, Ca.

> -----Original Message-----
> From:     Westh Stefan [SMTP:stefan.westh@celsius.se]
> Sent:     Tuesday, February 08, 2000 12:08 AM
> To:     'VEE reflector'
> Subject:     RE: vrf Debug help
>
> Hi Barrie!
> I think you have a problem with the Set Variable Object. Setting the
> variable name with a control input causes this behavior in HPVEE 5.01. See
> the attached example.
>
> Best Regards
>
> Stefan Westh
>
> Metrology/ RF & Microwave
> Laboratory Deputy Manager, RF & Microwave
> --------------------------------------------------------------------
> Celsius Metech AB
> MA H
> Box 1015
> SE-732 26 ARBOGA
> SWEDEN
> Tel +46 589 82640
> Fax +46 589 10740
> http://www.celsiusmetech.com
> mailto:stefan.westh@celsius.se
>
>
>
>
> -----Original Message-----
> From: Barrie Walden [mailto:bwalden@whoi.edu]
> Sent: den 8 februari 2000 01:36
> To: HPVee
> Subject: vrf Debug help
>
>
> Hi Folks,
>
> I have a lengthy Vee 5.01 program which seems to have a problem which I
> can't locate.  The program appears to execute correctly in a continuous
> loop but at some point within each cycle the cursor changes to an hour
> glass and the normal "running" message in the bottom left corner changes
> to some other message envolving line numbers.  Both of these things
> occur so quickly that they are hardly noticeable and I certainly can't
> read the lower left message.  I have tried slowing the program down with
> the debugging aids but there is no effect on the duration of the message
> in question - I still can't read it.  I have tried single stepping
> through the program but either the message doesn't appear or I have run
> out of patience before reaching the problem area.
>
> Does anybody have any suggestions?
>
> Barrie Walden
> WHOI
> ---------------------------------------------------------------------
> This is the "vrf" maillist, managed by Majordomo.  To send messages to
> this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
> unsubscriptions are done through the address "vrf-request@lvld.hp.com".
> If you need details, just send a message containing the text "help"
> to "vrf-request@lvld.hp.com".
> ---------------------------------------------------------------------
>  << File: set variable name.vee >>
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes