In message <c=SE%a=_%p=LG_PRODUCTS%l=LGP_AS1-970827100852Z-
1743@lgp_as1.lgp.se>, =?iso-8859-1?q?H=E5kan_Davidsson?=
<hakan.davidsson@lgp.se> writes
>Hallo!
>
>I have a calibration problem using components drives to an HP 8753 D.
Hello Hkan
Attached is a section of my utilation of the full two port cal for the
HP8753.
Unfortunately, it's deliberately incomplete out of respect for the
company for whom it was written.
One thing that I discovered is that you can put a function call into a
line inside a direct I/O object and, using this trick, I was able to
copy the HP-BASIC Full Two Port Cal routine from the Programmers manual
for the instrument. Instead of 50 or so direct I/O objects, there is
only a couple, one of which will have 50 lines or so when completed.
The userFunction "UserPromptAndConfirm" ( not included ) simply displays
the message and waits for the operator to hit a key to carry on.
I hope the attached program ( in HP-VEE Rev 3.12 ) will be of some help
to you.
Regards
1743@lgp_as1.lgp.se>, =?iso-8859-1?q?H=E5kan_Davidsson?=
<hakan.davidsson@lgp.se> writes
>Hallo!
>
>I have a calibration problem using components drives to an HP 8753 D.
Hello Hkan
Attached is a section of my utilation of the full two port cal for the
HP8753.
Unfortunately, it's deliberately incomplete out of respect for the
company for whom it was written.
One thing that I discovered is that you can put a function call into a
line inside a direct I/O object and, using this trick, I was able to
copy the HP-BASIC Full Two Port Cal routine from the Programmers manual
for the instrument. Instead of 50 or so direct I/O objects, there is
only a couple, one of which will have 50 lines or so when completed.
The userFunction "UserPromptAndConfirm" ( not included ) simply displays
the message and waits for the operator to hit a key to carry on.
I hope the attached program ( in HP-VEE Rev 3.12 ) will be of some help
to you.
Regards
I have a calibration problem using components drives to an HP 8753 D.
I want to make a full two port calibration whit a N-calkit, and
everything seems ok until youll select male or female port in the
reflection meny.
The comando I use is first "FULL2_S11_OPEN" after that I ping the
"FULL2_OPEN_MALE", now the NA just stops and after I while I get the
time out failure, on the output of the componentdrive I have the
commando "S11_OPEN_MEASURED"
Pleas help me am stuck.
Best regards / Hkan.
Hkan Davidsson, Production Enginnering, LGP Telecom AB
Tel: +46 8 624 43 46 Fax: +46 8 624 46 97 Mobil: +46 70 424 15 00
Email: hakan.davidsson@LGP.se