>
> From: mike.groves@ericsson.com
> To: VEE Reflector
> Subject: Multiple VEE's and won't Maximize
> Platform: Windows NT 4.0 on Vectra Pentium PC with VEE 4.0
>
> I've got two questions that are more annoyances rather than
> severe problems.
>
> First, I know NT and VEE both allow you to run multiple copies of
> the same VEE program at one time, so how does one defeat this added
> blessing? My program that production test runs, controls a good
> amount of expensive test equipment. The program expects the
> equipment states to be exactly where it put them without any
> extra time wasted re-checking. Running two or more programs at
> the same time, could prove disastrous.
>
> I guess one quick and dirty way would be to set an environment
> variable that SET's VEE=ON, or something like that and check for
> it when you run. But if a program is abnormally terminated it
> would not clear this and another copy would then refuse to go.
> Same with a temporary file used as a flag.
>
> Any other ideas? Can NT (or 95) itself be queried to find out
> if another VEE program is already running?
>
> And on a less important (but more irritating) subject, you offer
> start-up switches that can control the size and position of the
> window when it runs. I can find nothing to force VEE to MAXIMIZE
> its window. Is this difficult to implement or something?
>
> Also, RunTime has NO window position/size switches available at
> all, and worse yet, if I set Run Maximized in a shortcut properties
> box, VEE always overrides that and does what it wants anyway.
>
> Any plans for future enhancements along these lines?
>
> Thanks,
> Mike
Mike,
We had the same problem with test programs for flight hardware. This
solution worked but there may be better ways. Here goes.
1. Make sure the NT/DOS command utility Tlist.exe is on your system.
It will be found under winntsystem32. If it is not, you can get it
from a WIN NT 3.51 resource manager CD.
2. Create a .BAT file (call it tasklist.bat), it should contain the
following command:
tlist /b %1 > tasklist.txt
3. You can now execute tasklist.bat from VEE using the Execute Program
(PC) function.
4. Next, you can use a VEE Get File function to read the contents of
tasklist.txt. At this point if you have more than one VEE process
running it will appear in the list.
5. I captured all the vee.exe processes and parsed out their name field
and displayed a message to the operator strongly suggesting that under
no circumstances he/she should run a test and that Software Engineering
should be notified.
This approach worked for us, of course it's up to you how you handle
multiple processes...
good luck.