AnsweredAssumed Answered

Delete globals at prerun

Question asked by VRFuser on Jul 16, 1997


1.  VEE 4.01 Development environment has a DELETE GLOBALS AT PRERUN option
in the default preferences menu.  What affect does this have in the 4.0 RUN
ONLY (vxe) environment?  Is there a PRERUN condition with the 4.0 RO
environment?

2.  We have quite a few programs that were developed in VEE 3.12  ---> We
were storing some "flag" variables in globals.  These flags consisted of
stuff like Test Count, Test results (PASS, FAIL, NOT TESTED, etc).  When
porting these programs over to VEE 4.01 (Compatibility mode= CHECK), they
work fine EXCEPT that the Runonly environment doesn't handle errors the same
way.  When an error is encountered, it brings up the ERROR Message box, and
the OK button terminates the program.  Is there ANY way around this other
than revising my programs?  If not, then I suggest that you change the OK
button to say "PROGRAM TERMINATED".

3.  Can we get the EXECUTE PC object to execute a VXE program?  If yes then
How?

Thanx,

Jeff Davis - Rev 33.00

Outcomes