AnsweredAssumed Answered

HpVee in Startup?

Question asked by VRFuser on Jul 17, 1997
Dear HpVee users,

After putting Hpvee (V3.21) in the Windows 95 start up  with the command
'-r', I managed to load and run my Vee program when there is rebooting
(after an electricity cut, for example). However, after emerging, the
toolbars of Hpvee do not appear and I cannot manage to deal with the
program. The only way I can stop the program is by forcing an error to occur.

Does anyone know how we can load the Vee toolbars with a simultaneously
running program? 

Thanks in advance

Nuno Moreira
-------------------------------------
Nuno Moreira
DER-ITE-INETI
-------------------------------------
e-mail  : nuno.moreira@ite.ineti.pt
Address : Estrada do Pao do Lumiar
          1699 Lisboa Codex
          Portugal
Tel.    : 351.1.7162712/5141-Ext.2730
Fax.    : 351.1.7163797
-------------------------------------


Outcomes