AnsweredAssumed Answered

VRf-VEE_Questions

Question asked by VRFuser on Jul 17, 1997
send q VRf-VEE_Questions ww gleissner_a vrf

from: Greg Goebel / HP-MXD
      gvg@lvld.hp.com / 970-679-3030 / FAX 970-679-5971
to:   VRf-Dr. Albert Gleissner
date: Friday, 18 July 1997 0940 MDT

> Date: Thu, 17 Jul 1997 16:07:09 +0200
> From: "Dr. Albert Gleissner" <seminar@meilhaus.de>
> Organization: Meilhaus Electronic
> To: "VEE Reflector (VRf)" <hpvxd_xc@hpislsup.lvld.hp.com>
>
> Hi folks,
>
> there are two questions/problems I hope to get some support from
> anybody:
>
> 1. Has anybody experience, example programs, literature etc. for
> programming ActiveX communication with HP VEE 4.0 ?

We're still trying to figure this thing out in support and document it
ourselves.  The relevant engineer transferred to another division and
people are on vacation, so we are having some (temporary) problems getting
assistance on it ourselves.  Once we do get it working, we'll try to document
it neatly and publish it in Exchange.

> 2. A concrete problem with HP VEE 3.12: To an UserObject with panel, a
> "Print" Control-Terminal is added, connected to a toggle control.
> Pressing the toggle-button, the panel is printed out. Executing this
> program with the full developing version, it works fine. =
>
> But trying to execute the same function using the Run-Only Version, it
> doesn=B4t work.
> Does anybody know why ???

I tried this on VEE 3.12 with a simple program and it worked fine.  One
variation, however, was that I didn't have VEERUN installed on that PC
so I used the "-r" option, which is equivalent.

> Thanks and regards
> Albert Gleissner
>

Outcomes