AnsweredAssumed Answered

vrf AW: Serial Timeout error

Question asked by VRFuser on Nov 12, 2003
The problem already exists after using Xon/Xoff handshake. Is there a problem with VEE? Or is it possible that the serial port causes all these problems?
I have no other chance talking to the control equipment. What else can I do, improving the connection?

-----Ursprngliche Nachricht-----
Von: LOPEZ,PACO (HP-Spain,ex2) [mailto:paco.lopez@hp.com]
Gesendet: Donnerstag, 13. November 2003 12:19
An: Abraham Mario
Betreff: RE: [vrf] Serial Timeout error


Is it a must to use no handshaking in your app??. I asked you because the
handshaking improves and makes sure the communication. Try using the
Xon/xoff.

-----Original Message-----
From: Abraham Mario [mailto:M.Abraham@lasercomponents.com]
Sent: Thursday, November 13, 2003 12:12 PM
To: LOPEZ,PACO (HP-Spain,ex2)
Subject: AW: [vrf] Serial Timeout error


no handshaking (none).

-----Ursprngliche Nachricht-----
Von: LOPEZ,PACO (HP-Spain,ex2) [mailto:paco.lopez@hp.com]
Gesendet: Donnerstag, 13. November 2003 11:39
An: Abraham Mario
Betreff: RE: [vrf] Serial Timeout error


Which handshaking are you using for the serial communication????

-----Original Message-----
From: Abraham Mario [mailto:M.Abraham@lasercomponents.com]
Sent: Thursday, November 13, 2003 9:12 AM
To: VRF
Subject: [vrf] Serial Timeout error


Hello together,

Im using VEE Onelab 6 to create a automatic measurement. Via Serial
Interface I try to make some settings and also get some information about
the serial connection. If the dataflow is very high, I sometimes get a
timeout error. And if I activate the SHOW EXECUTION FLOW and/or SHOW DATA
FLOW Button the program runs better.
Did anybody know about this problem. Is the serial connection not suitable
for this or shoult I make special settings in the I/O menue.

Thanks for you answer.

best regards,

Mario Abraham


LASER COMPONENTS GmbH
Werner-von-Siemens-Str. 15
82140 Olching
Phone:     +49 (8142) 2864 - 45
Fax:     +49 (8142) 2864 - 11
mailto:m.abraham@lasercomponents.com
http://www.lasercomponents.com


---
You are currently subscribed to vrf as: paco.lopez@hp.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes