AnsweredAssumed Answered

VRf-Need help...

Question asked by VRFuser on Jun 9, 1997
Thanks to all for a VERY prompt response to my problem with an
instrument driver for the antique signal multiplexer (accepting only
bytes from 0 to 12 as channell codes). Of course, it works very fine
with direct I/O (there is no problem with addressing). It even works
with a dummy instrument driver (which does nothing but a standard
serial pooling) which I have prepared.

Unfortunately I HAVE TO WRITE THE INSTRUMENT (PANEL) DRIVER (in spite
that I do not wont to and see any sens of doing this ...).

Any further suggestions ?

Pawel Zylka
Institute of Electrotechnics and Electrotechnology
Wroclaw Technical University
zylka@elektryk.ie.pwr.wroc.pl
pzy@heaven.anest.am.wroc.pl

Outcomes