AnsweredAssumed Answered

driver of TEKTRONIX AWG2021

Question asked by VRFuser on Jul 28, 1997
Dear Sirs,

we are  searching for HP-VEE instrument driver (.id) of
TEKTRONIX AWG2021 arbitrary waveform generator.

Needed Features:
         Reset AWG,
         load HP-VEE waveforms directly to AWG waveform-files,
         load HP-VEE array directly to AWG sequence-file,
         set AWG parameters (both channels),
         run function generator.

It would be great if the output of the AWG is displayed
in the HP-VEE panel.

thanks in advance
 
best regards


--
===================================================
  Andreas SCHWARZ
  Dipl.-Ing.
  Electrical Design
  Design Engineer

  AUSTRIAN AEROSPACE Ges.m.b.H.
  Breitenfurter Strasse 106-108
  A-1120 Vienna, AUSTRIA / EUROPE

  Tel.  : +43-1-80199/5546
  Fax   : +43-1-80199/6950
  E-Mail: andreas.schwarz@space.at
  IEEE Member No: 40177594
====================================================
  This email is for information only!
====================================================

Outcomes