In message <c=SE%a=_%p=LG_PRODUCTS%l=LGP_AS1-970827100852Z-
1743@lgp_as1.lgp.se>, =?iso-8859-1?q?H=E5kan_Davidsson?=
<hakan.davidsson@lgp.se> writes
>Hallo!
>
>I have a calibration problem using components drives to an HP 8753 D.
Hello Hkan
Attached is a section of my utilation of the full two port cal for the
HP8753.
Unfortunately, it's deliberately incomplete out of respect for the
company for whom it was written.
One thing that I discovered is that you can put a function call into a
line inside a direct I/O object and, using this trick, I was able to
copy the HP-BASIC Full Two Port Cal routine from the Programmers manual
for the instrument. Instead of 50 or so direct I/O objects, there is
only a couple, one of which will have 50 lines or so when completed.
The userFunction "UserPromptAndConfirm" ( not included ) simply displays
the message and waits for the operator to hit a key to carry on.
I hope the attached program ( in HP-VEE Rev 3.12 ) will be of some help
to you.
Regards
1743@lgp_as1.lgp.se>, =?iso-8859-1?q?H=E5kan_Davidsson?=
<hakan.davidsson@lgp.se> writes
>Hallo!
>
>I have a calibration problem using components drives to an HP 8753 D.
Hello Hkan
Attached is a section of my utilation of the full two port cal for the
HP8753.
Unfortunately, it's deliberately incomplete out of respect for the
company for whom it was written.
One thing that I discovered is that you can put a function call into a
line inside a direct I/O object and, using this trick, I was able to
copy the HP-BASIC Full Two Port Cal routine from the Programmers manual
for the instrument. Instead of 50 or so direct I/O objects, there is
only a couple, one of which will have 50 lines or so when completed.
The userFunction "UserPromptAndConfirm" ( not included ) simply displays
the message and waits for the operator to hit a key to carry on.
I hope the attached program ( in HP-VEE Rev 3.12 ) will be of some help
to you.
Regards