AnsweredAssumed Answered

VRF-Beep

Question asked by VRFuser on Mar 25, 1998


/ Beep Limitations As Of VEE 4.0 /

* The Beep Object doesn't work all that well on Win32 under VEE 4.X or later.
It sometimes only gives a faint click and frequency can't be controlled at
all.  The reason is that Microsoft settled on an API call that doesn't
provide much in the way of control and so it's difficult to work around.
Using a sound card and a WAV player is the best option over the long run.

[<>] gvg

Outcomes