<!DOCTYPE HTML PUBLIC "-//W3C//DTD W3 HTML//EN"><HTML><HEAD><META content=text/html;charset=iso-8859-1 http-equiv=Content-Type><META content='"MSHTML 4.71.1712.3"' name=GENERATOR></HEAD><BODY bgColor=#ffffff><DIV><FONT color=#000000 size=2>Hi all,</FONT></DIV><DIV><FONT color=#000000 size=2></FONT> </DIV><DIV><FONT color=#000000 size=2>I've got, what I hope, a simple question. During a test I want to create an emergency stop. But when VEE is busy with Acquisition I can not interrept!</FONT></DIV><DIV><FONT size=2>Using a switch or something like that doesn't work. The biggest problem for me is that a certain analogue output stays high. So when a test is roughly interrepted the main control point still receives power (10 Vdc)! Is there a possibility to give a certain function or switch the highest priority? Or is there a possibility to stop the analogue output (smoothly)?</FONT></DIV><DIV><FONT size=2></FONT> </DIV><DIV><FONT size=2>Thanks,</FONT></DIV><DIV><FONT size=2></FONT> </DIV><DIV><FONT size=2>Arjan</FONT></DIV></BODY></HTML>