AnsweredAssumed Answered

VRF - RunTimeOnly Help Request

Question asked by VRFuser on Feb 9, 1998
>      FROM:
>    michelle.farris@stellexms.com
>    Michelle Farris
>    3333 Hillview Ave
>    Palo Alto, California, USA
>    650-813-2279
>    re:  VRF - RunTimeOnly Help Request
>      ****
>      I am developing a user interface (Vee 4.01, Win95) which allows the
>      user's computer to set up various parameters on an HP Pulse
>      Generator HP8112a.  I developed the program at my computer,
>      installed RunTimeOnly Vee from the CD onto the user's computer
>      which is also Win95.  When I run the program on my computer, all is
>      well.  When I run it on the user's computer I immediately receive
>      an error "Invalid Device Encountered - Error #904 - Parse Error".
>     
>      I have copied the vee.io file from my computer, where the device IS
>      configured, to the user's computer and still receive the same error
>      message.  Any idea's or suggestions??? 
>     
>      Thank you,
>      Michelle

I had an error similiar to that a while ago, and it turned out not to
be in one of the devices at all.  What had happened was that I was
using a reserved word for an input into a user function (the word was
Err, actually) and it would not load properly.

Once I changed it to E_rr everything worked fine.

I'd check that if I was you...


    _
   /      Greg.Noseworthy@comdev.ca
  / __    ComDev
/ / _    -----------------------------
(_/_/___)  "Lost In Space" Group

Outcomes