AnsweredAssumed Answered

Vrf - Active X Automation Server w/in VEE?

Question asked by VRFuser on Nov 3, 1997

     Is it possible to call an Active X Automation server directly from
     VEE?
    
     My application is to write into a database directly from VEE. Is this
     possible? I noticed a reply from one user who writes out ascii files
     and then imports them into the database.
    
     The other option I can think of is writing a DLL that does it and call
     it from within HPVEE.
    
     A colleague of mine has an Active X object that will do it directly,
     but I'm not sure if it can be done from w/in VEE.
    
     Thanks,
    
     /Susan Cudmore
     Chiron Diagnostics
    
    
    

Outcomes