Hello,
I am trying to use one computer to control two other computers via Hpvee
program.
I want to set up the other two like an instrument and control them from the
main computer.
Is this possible thru Gpib or will I have to network them together?
Thanks for any suggestions.
Nick Dottellis
EE Tech
AlliedSignal
I am trying to use one computer to control two other computers via Hpvee
program.
I want to set up the other two like an instrument and control them from the
main computer.
Is this possible thru Gpib or will I have to network them together?
Thanks for any suggestions.
Nick Dottellis
EE Tech
AlliedSignal
> Hello,
>
> I am trying to use one computer to control two other computers via Hpvee
> program.
> I want to set up the other two like an instrument and control them from the
> main computer.
> Is this possible thru Gpib or will I have to network them together?
>
> Thanks for any suggestions.
>
> Nick Dottellis
> EE Tech
> AlliedSignal
Sir:
You do NOT want to do this with HPIB/GPIB. VEE has no way of
reading or writing data if it is not an HPIB controller.
However, communicating between VEEs using To/From Socket
over a LAN is remarkably clean.
[<>] regards -- greg goebel