Hi All,
Just a quick question ...
Is there the facility to give the showPanel function ONLY the Panel size, and not the position ?
If not, is there a way to show the Panel in the center of the screen (with a specified size) ?
< Or even get the size of the resolution the PCs running in >
I'm running Vee 4.01 under Windows 95.
Thanks
James
(James.Atkin@Phase.Com)
Just a quick question ...
Is there the facility to give the showPanel function ONLY the Panel size, and not the position ?
If not, is there a way to show the Panel in the center of the screen (with a specified size) ?
< Or even get the size of the resolution the PCs running in >
I'm running Vee 4.01 under Windows 95.
Thanks
James
(James.Atkin@Phase.Com)
> Hi All,
>
> Just a quick question ...
>
> Is there the facility to give the showPanel function ONLY the Panel size, and not the position ?
As per the online help, you have to specify position if you specify panel size.
> If not, is there a way to show the Panel in the center of the screen (with a specified size) ?
Only by specifically positioning it there.
> < Or even get the size of the resolution the PCs running in >
Not with VEE itself. For VEE 5.0 we may be able to find or make ActiveX
Controls to do that job.
> I'm running Vee 4.01 under Windows 95.
>
> Thanks
>
> James
>
> (James.Atkin@Phase.Com)
[<>] regards -- gvg