AnsweredAssumed Answered

VRF - help with counter object

Question asked by VRFuser on Jun 22, 1998
Re: VRF need help with counter object.

Hi,

I'm trying to count the number of times that I go through each of two loops
using the counter object.  After cycling, I then want to display the number
of times I went through each loop.

The problem, if I cycle in only one of the loops, the other is "zero".  The
display in the counter shows zero, but its output is "nill" and does not
display on any output device.

I want the output to be zero, not "nil" so that I can add the two counters
for
a total number of cycles.

How can I fix this?

Thanks

Wally
czubatyj@ovonic.com  (248)-280-1900 x 6106

Outcomes