Hello,
I am running HP VEE 5.01 on Windows 98. It is only the gpio that causes
problems, if the data is transferred over the hpib there are no problems.
Right now, I give the voltmeter a set number of readings that it is
suppose to transfer on each trigger. The first trigger works fine, and the
data is collected, but on subsequent triggers a timeout occurs.
Thanks,
Gordon Rueff
I am running HP VEE 5.01 on Windows 98. It is only the gpio that causes
problems, if the data is transferred over the hpib there are no problems.
Right now, I give the voltmeter a set number of readings that it is
suppose to transfer on each trigger. The first trigger works fine, and the
data is collected, but on subsequent triggers a timeout occurs.
Thanks,
Gordon Rueff
I am using a 44074 high speed voltmeter in a 3852a, and transferring the
readings over the voltmeter's GPIO connection. I have a program that works
once, but to take more than one set of reading I must reset the voltmeter
and reload the VEE program. I am also using the GPIO to trigger the
voltmeter. Does anyone have any ideas why I can not take more than one set
of readings each time I load my program.
Sincerely,
Gordon Rueff