AnsweredAssumed Answered

VRF NI repeat addressing

Question asked by VRFuser on Jun 2, 1998
VRF,

I'm using HP Vee 4.0 with a AT-GPIB/TNT NI card under WIN95.
For one instrument I need to set the repeat addressing to enable.
>From C of Basic I would send the following command

Ibconfig (device, IbcREADDR, 1)

How can I send this command from HP VEE ?

Michel Cyr
Nortel
ph 613-765-2634
fx 613-765-2471

Outcomes