AnsweredAssumed Answered

vrf Web Monitoring

Question asked by VRFuser on Apr 19, 2000

Lee,

I did experience some problems at first when I enabled the VEE
web-monitoring feature. The problem was when I tried to exit VEE, VEE would
stop responding and I would have to kill it through Task Manager. The easy
solution is to change the port that VEE uses for http transactions from 80
to something else. Then in the web browser connect to that port specifically
using http://myserver.com:90 (if port is changed to 90). The http standard
connection port is 80 and Personal Web Server is set by default to the same
port. When I made this change, I had no more problems.

Hope this helps,

Lyle Carnahan
Agilent Technologies


-----Original Message-----
From: HUDSON,LEE (HP-SanJose,exgen1) [mailto:lee_hudson@am.exch.hp.com]
Sent: Wednesday, April 19, 2000 6:40 PM
To: 'vrf@lvld.hp.com'
Subject: vrf Web Monitoring


Hi Everyone,
Has anyone experienced a problem with Microsoft's Personal Web Server (PWS)
application interfering with Web Monitoring (re: VEE 5.0)?
Thanks,

Lee Hudson, Hardware Engineer
LumiLeds Lighting, U.S., LLC
370 West Trimble Road, MS 91UH
San Jose, CA 95131
(408) 435-5834
(408) 435-6574
lee_hudson@agilent.com
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes