AnsweredAssumed Answered

vrf AW: Time Domain

Question asked by VRFuser on Mar 12, 2000
Hi Stan,

I programmed a HP 8510C to read out different images. Therefore I build a
function with the following command sequence with Direct I/O.

DOMA?           to get, if it is Time or Frequency Domain
STAR;OUTPACTI;  to get the start value of time or frequency
STOP;OUTPACTI;  to get the stop value of time or frequency
Write Text "FORM3;OUTPDATA;"EOL
READ BINBLOCK x REAL64 ARRAY:*,2   to read the data array

The data array consists of two dimensions, one for the imaginary and one for
the real part. Out of this arrray and with the start- and stop time or
frequency value I can build the desired array of time and amplitude or time
and phase. I'm not sure that this is what you want, but perhaps it will
help.

Jens


--------------------------------------------
Dipl.-Ing. Jens Fischer      

SOMATEC - Software fr Maschinensteuerungen
und Automatisierungstechnik GbR

Jagdweg 7a
D-82041 Deisenhofen

Tel.:     (089) 613 984 93
Fax:      (089) 613 981 23
E-mail:   Fischer@somatec.de
Homepage: http://www.somatec.com
--------------------------------------------



> -----Ursprngliche Nachricht-----
> Von: owner-vrf@hplvlrx.lvld.hp.com
> [mailto:owner-vrf@hplvlrx.lvld.hp.com]Im Auftrag von Stan Bischof
> (Richard S)
> Gesendet: Freitag, 10. Mrz 2000 19:03
> An: vrf@lvld.hp.com
> Betreff: vrf: Time Domain
>
>
> Before I dig into the details---
>
> Has anyone built a VEE program to convert measured S parameter
> data to time domain (step TDR) format? Basically reproduce the
> existing time-domain conversion that occurs in network analyzers
> like the 8510.
>
> I'm familiar with the general steps needed but wouldn't mind
> a completed example!
>
> thanks
>
> Stan
>
>
> ----------------------------------------------------------------------
> Stan Bischof  Agilent Technologies       707-577-3994    rsb@sr.hp.com
> ----------------------------------------------------------------------
> ---------------------------------------------------------------------
> This is the "vrf" maillist, managed by Majordomo.  To send messages to
> this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
> unsubscriptions are done through the address
> "vrf-request@lvld.hp.com".
> If you need details, just send a message containing the text "help"
> to "vrf-request@lvld.hp.com".
> ---------------------------------------------------------------------
>
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes