AnsweredAssumed Answered

vrf VEE / Access files

Question asked by VRFuser on Mar 12, 2000
Attached is a zip file containing two files:

1) ActiveX_Userfunction_desc.doc -- contains written documentation for all
userfunctions and userobjects in accompanying .vee file.

2) ADO_library.vee -- contains several userfunctions and userobjects used to
interact with Access from VEE.

Note that I am using ADO 2.1(ActiveX Data Objects) and Jet 4.0 (the Access
database engine).  Both of these upgrades are available for free from
Microsoft.  See http://www.microsoft.com/data/download.htm.  It's possible
you can use lower revisions by changing the references as needed.  (I was
using Jet 3.5 until recently.)

Finally, in a shameless act of self promotion, I am available for
programming.  See http://www.techinfosystems.com for more info.

Good luck!

Roger Martin

Outcomes