AnsweredAssumed Answered

vrf Access ActiveX - Tables

Question asked by VRFuser on Jul 19, 2000
The SQL statement that creates the table would be the same, but the syntax
used to transmit it to Access would be quite different.  Unfortunately, I
don't remember enough about DAO to be able to convert it.  Sorry.

Roger Martin
Applications Programmer
www.techinfosystems.com

-----Original Message-----
From: Graeme Hickey [mailto:graeme@pixelfusion.com]

Thanks for the help, Im using  DAO.DBEngine.35 from Vee I take it the
command structure
Would be the same?

Regards
Graeme
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes