AnsweredAssumed Answered

vrf An HP E2050A Problem.

Question asked by VRFuser on Apr 28, 2000
Cagri,

Telnet to your E2050A gateway using its IP address.  Two configuration
parameters that it uses are:

  lan-timeout
  io-timeout

If the value is set to 0, there is no timeout.  I have mine set to what I
believe to be the default settings which are:

  lan-timeout    0
  io-timeout    15

I have not had any problems or timeouts with these settings.  Take a look
and try these values.

                         Tom Romalewski
                         Lucent Technologies
                         Holmdel, NJ  USA

                         VOICE:  (732) 949-6202
                             E-MAIL: romalewski@lucent.com


----- Begin Included Message -----
-----------------------------------------------------------------------
Hello everybody,
I use an HP E2050A in order to control an HP 34970 via network. When I
start Vee and load the test program, it works fine. But when I do not use
the same program for a while (for example half an hour) and when I try to
re-run the application, it says that "Lock Aquisition failed on HP-IB
interface hpib7 on 2050_IP" and the error code is 814. When I close the
session and re-open it, it is again ok.
I think the 2050 causes this error. I don't know how to overcome this
problem. I fear that in case my test program runs very long, after a while
I may see this error window that terminates the whole test program.
Is there a time-out setting or something else for such a problem?

Any help would be appreciated.

-----------------------------------------------------------------------

Cagri Acar
Mikro Dalga ve Sistem Teknolojileri / Microwave and System Technologies
Elektrik Donanim Test Birimi        / Electrical Equipment Test Unit
ASELSAN A.S.
PK 101 Yenimahalle Ankara/Turkey

Phone:+903123851900-2701

----- End Included Message -----

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes