Hi, all,
I need to simulate the geometry as shown in the following figure.
Is it possible to draw this ribbon like geometry?
Thank you very much
Yours,
Yiliu
I need to simulate the geometry as shown in the following figure.
Is it possible to draw this ribbon like geometry?
Thank you very much
Yours,
Yiliu
1) draw a cylinder, (cross section (X-Z) being a circle, extrude in Y direction)
2) cut the cylinder two heads parallelly, with the cut NOT vertical to Y direction ( X-Z cross section changed to ellipse)
3) cut a small portion of the bottom (X-Z cross section ellipse will be partly curve of ellipse + one line connecting the two heads of the curve)
4) make a sheet body of the geometry round face
5) Connect two sides of the sheet completed in step 4 to the footprint with sheets
thank you all!