AnsweredAssumed Answered

Missing settings in Golden Gate?

Question asked by shadi.michael on Jun 1, 2010
Hello,

I am missing some settings in Golden Gate that I used to have in RFDE when setting a harmonic balance simulation:

[1] Setting the status level to determine the amount of information that shows in the simulation report.

[2] Setting the name of the output ADS dataset (*.ds file). The default I get now in Golden Gate is schematic_CR.ds

Anyone knows if these are still available somewhere?

Thanks.

/Shadi  

Outcomes