AnsweredAssumed Answered

vrf Short beep message

Question asked by a.kieser on May 17, 2000
Thank you for your frequent answers and good ideas, but...

The solution with using the beep-function of kernel32.dll doesn't work
because I'm running Windows 98. Any Solution using a .wav-file takes too
much time (there must be beeps with 300ms or less...).
Any other ideas, perhaps a beep.dll, which is working under win 95 so I can
send a beep with my own duration and frequency?

My problem was to send out frequent beeps triggered from a high / low-signal
with HP Vee 5.0

Thanks in advance,
Axel Kieser


**********************************************************************
This email message has been swept by MIMEsweeper for the presence of
computer viruses.

Francotyp-Postalia AG & Co.

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes