AnsweredAssumed Answered

VRF- VISA Attributes

Question asked by VRFuser on Aug 26, 1999
Hi all,
is anybody there experienced in writing VISA applications ?
I've written a driver for a register based VXI device based on a HP
E1490 breadboard. But I'm unable to use the viSetAttribute function
to define a device timeout ( VI_ATTR_TMO_VALUE ). I compared
the function call with the VXI PNP source files from HP, but the
only difference I see is that these devices are message based.
Is a manual available for writing VXI PnP driver ?

Many thanks in advance for any help.
Regards

Christian

Biotronik GmbH & Co
Woermannkehre 1
D 12359 Berlin - Neuklln
Tel.: +49 30 689 05 - 301
--------------------------------------
christian.wienhold@biotronik.de
--------------------------------------


Outcomes