AnsweredAssumed Answered

Amplicon pc263 switch card DLL

Question asked by VRFuser on Feb 15, 1999
Hi
The card is using the default base address of 300 hex and works fine
with the supplied visual basic interface that calls the DLL files used
below?
I am trying to use the switch card DLL under VEE 5.01
I am using the Import library function
this has the call to the DLL pc263dll.dll
and the call to the .h file pc263dll.h
Both files have been put in the windows system directory to ensure that
they are in the
path.
Vee gives the error message cannot load DLL system error code 0x1F(31)
device attached to the system is not functioning
ERROR 716
Any ideas?
Regards Mike

Phone +44 (0)1908 221344         M/A-COM Ltd 
Fax     +44 (0)1908 221366         Featherstone Road
mstrutt@amp.com                       Wolverton Mill
Principal Test Engineer                Milton Keynes
                                                 MK12 5EW
A little learning is a dangerous thing.
Drink deep, or taste not the Pierian spring.
(Alexander Pope 1688-1744)


Outcomes