AnsweredAssumed Answered

VRF-User control interface devices

Question asked by VRFuser on Jan 27, 1999
Roufosse, Gary wrote:

> Can someone please indicate where I could glean further information on
> utilizing different user control objects withing HP-VEE, i.e., LED's,
> switches, etc. Are such objects available and usable within the UI?

As far as this request goes, that sounds like the toggles.  If you
want a custom toggle, you can specify "custom" in the default preferences
for the toggle and specify two GIF bitmaps for the "on" and "off" state.

If you want more sophisticated UI stuff, there's been a bit of tinkering on
various ideas, not all of it very clean.  Some specifics would be needed on
what is desired.

[%%] regards -- gvg

Just a suggestion:  please remember to use the "VRF-" suffix as a courtesy
to other VRF users.

--
    Greg Goebel          ftp://fcext3.external.hp.com/dist/mxd/index.html
    HP MXD Marketing     http://hpislsup.lvld.hp.com (HP only)
    pctm@lvld.hp.com     http://www.geocities.com/CapeCanaveral/Launchpad/6000

Outcomes