AnsweredAssumed Answered

VHF. dmm 34401A

Question asked by VRFuser on Jan 28, 1999
Hello,

Hopefully this is a simple question.  I am taking the min and max readings from the DMM, but in part of the test they need to
read the display manually to adjust a trimpot I want the display to have only two digits after the decimal and it has to go slow
enough for them to read the DC Voltage.  Every time I switch it to only 2 places it speeds up two fast to read.  Is there another
way to change it than to use Write text "conf:volt:dc 100,.01;" EOL?  I went through the book but ended up a little confused.

Thanks for the help,

Scott Anderson
Process Development
ADC Solitra
Hutchinson MN
Scott_Anderson@ADC.com
(320) 234-7612


Outcomes