AnsweredAssumed Answered

simultaneous excecution, Network analyser and motor control

Question asked by VRFuser on Aug 13, 1999
Hello,

I am using a sequencer to sequence a series of tests. When I am done I
build a record.

Input to the record is:
timestamp
serial no
operator no
job no
and from the sequencer - test results with pass/fail= 1/0.

Then I do a 'tofile', then 'fromfile'.
When I open the file in wordpad I get alot of information that is hard to
read.

Is there a way to organize the data?
i.e, add a space between each test?
create name fields and put the data under those fields?

Also, can I make it say "pass/fail" instead of 1/0 in the record coming
from the sequencer?

any help is appreciated

thanks

Outcomes