AnsweredAssumed Answered

8753 network analyzer

Question asked by VRFuser on Sep 23, 1999
Hello Scott

Try 'OUTPSERN'.

---
Jens Johnsen
Production Engineer
Celwave R.F. A/S
Frejasvej 30
DK 3400 Hillerd

Switchboard: (+45) 48 22 36 36
Fax:         (+45) 48 22 37 37
Direct:      (+45) 48 22 36 85
Email: jens.johnsen@celwave.dk

----------
From:    Anderson, Scott
Sent:    24. september 1999 13:41
To:    'vrf@lvld.hp.com'
Subject:    vrf:  8753 network analyzer

hello all

When using and 8753 network analyzer I can read the identification with "IDN?;", but does any
one know of a way to read the serial number or something else that I can use to keep each analyzer unique?

thanks

Scott Anderson
Process Development
ADC Telecommunications
BCG Wireless
1100 N 4th St.
Le Sueur, MN 56058
1-800-366-3889 EXT.4784
scott_anderson@adc.com

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes