AnsweredAssumed Answered

vrf Formula with control input

Question asked by VRFuser on Nov 10, 1999
With the GetCommandLineA of the kernel32 DLL you can get the command line
options of you VEE program.

I would not recomment to expand the entries in instrument manager. Is slows
down your application extremely. In the past we had a project that runs on
my computer about 10 times slower than on the other computers in our
company. I solved the problem in deleting all unused entries in the
instrument manager.

Best regards
B. Aufenanger

------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen

Telefon          : (089) 613 984 91
Fax.               : (089) 613 981 23
Email             : Aufenanger@somatec.de
homepage     : http://www.somatec.com
------------------------------------------------------------

-----Original Message-----
From:     owner-vrf@hplvlrx.lvld.hp.com [mailto:owner-vrf@hplvlrx.lvld.hp.com]
On Behalf Of Gustin Mike
Sent:     Wednesday, November 10, 1999 6:34 PM
To:     HPVee (E-mail)
Subject:     vrf Program Identification?

Is there anyway for a program to identify what vee.io library it is using?

I am starting up four instances of the same program with four different IO
libraries, via the command line option. I would like each program to
identify
itself based on the vee.io library that it is using.

If someone else can suggest another way without making the program unique
such as via the geometry offset or what ever, I am all ears.

Mike Gustin
Mike.Gustin@emg.sms.siemens.com
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes