AnsweredAssumed Answered

Overriding default timeout on HPIB.

Question asked by VRFuser on Jun 17, 1999
You can create a new instrument in the manager, which may use the same
driver but with a long timeout for example (ie: Spectrum Analyzer XY long
TO@709).
Now you can use this Instrument whenever you want to make measurements where
you need to have a long timeout.
The only possibility to read the current setting of the timeout I am aware
of, is to read the vee.io file and interpret it.

----- Original Message -----
From: <Jens.JOHNSEN@CELWAVE.DK>
To: <hpvxd_xc@hpislsup.lvld.hp.com>
Sent: Friday, June 18, 1999 9:01 AM
Subject: Vrf: Overriding default timeout on HPIB.


> I want to set the timeout for HPIB objects explicitly in some cases.
> I then use the Timeout control input in the direct I/O object.
> BUT I want to keep the DEFAULT timeout set in the Instrument manager for
those objects where I do not use the Timeout control input.
>
> To my surprise, using the Timeout control input seems to set the default
timeout  in the instrumentmanager. Is this really so?
>
> In that case I suddenly have to account for timeout in all objects
everywhere in my program. Also I can not rely on the timeout set in the
instrument manager when starting another program. If I have to save changes,
this also implies setting the the default timeout to the value last used in
this particular program.
>
> How do I keep the default timeout?
Georg Nied
Software Development
51149 Koeln
Germany
gn-software@gmx.de
ICQ 23490440



Outcomes