AnsweredAssumed Answered

vrf...excel_activex

Question asked by VRFuser on Jul 22, 1999
Hello all,

     I have two pc's. One is a HP Omnibook 5000 and one a clone. I've
written a program using
the same basic excel setup as in the excel97a activex example in vee.  My
problem is, on the Omnibook it works great, excel loads and the data is
transferred. On the clone, I keep getting an
error stating excel rejected the call. If I open excel first then minimize
it, the Clone program will work.  It's acting like I have a getobject
instead of createobject in my code.  Can anyone help?

Thanks in advance,

Todd

Outcomes