AnsweredAssumed Answered

OPENS/SHORTS CORRECTION TEST

Question asked by VRFuser on Jul 23, 1999
HELLO,

I have a lcr meter 4263B for measuring impedance. I have to prompt the
operator to perform an open/shorts correction test before and after
measuring capicatance and inductance. 

When a opens test is performed the displays reads "open correction complete"
when the leads are left open and if the admittance is less than 100uS
.
but if the leads are shorted when suppose to be open the display reads
"range out of limit"

In my vee program, I trust the operator is always going to perform the o/s
test correctly. (not always the case)

How do I "read" the measured value of the o/s correction test?
IF I can than I can compare that value to a constant and then display to
the operator if he/she performed the test correctly.

Thanks

Outcomes