AnsweredAssumed Answered

vrf Problems with short delays

Question asked by aufenanger on Jul 24, 2000
Hi Axel,

what you see is the minimum delay time of your operating system. In windows
95/98 you will see it as 55 ms. If you really want smaller times you will
need a hardware solution. If the time does not have to be absolutely exact,
you can use a defined loop. But here you will never have the guarantee for a
exact delay time.

Best regards
B. Aufenanger
------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen

Telefon          : (089) 613 984 91
Fax.               : (089) 613 981 23
Email             : Aufenanger@somatec.de
homepage     : http://www.somatec.com
------------------------------------------------------------
-----Original Message-----
From: owner-vrf@lvld.agilent.com [mailto:owner-vrf@lvld.agilent.com]On
Behalf Of a.kieser@francotyp.com
Sent: Monday, July 24, 2000 11:51 AM
To: vrf@lvld.agilent.com
Subject: vrf Problems with short delays

Hi there,
I have a problem if I try to get a very short delay within a Vee5-Program:
If I use the Delay-Device there seems to be a minimum time (on my NT4 -
166MHz-Pentium of about 10ms) for the delay - independent what I want to
have. A delay realized with a For-Count-Device can become much more shorter
(of about 0.04ms!).
Bug or feature?
Any suggestions to solve this Problem?
An example is attached.

With best regards,
Axel Kieser
___________________________
Francotyp-Postalia AG & Co.
TEZ - Technology Centre
Triftweg 21-26
16547 Birkenwerder
Germany
Tel.: +49 (0) 33 03/5 25 - 6 37
Fax: +49 (0) 33 03/5 25 - 6 49
mailto:a.kieser@francotyp.com
http://www.francotyp.com/

<<Delay.vee>>

**********************************************************************
This email message has been swept by MIMEsweeper for the presence of
computer viruses.

Francotyp-Postalia AG & Co.
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes