> I feel like I should pay you for this one. Heck, I have trouble gettin paid for the stuff I'm sposta get paid for! > I have a lot to absorb. It sure can be bizarre. Taken in small chunks, it does start to make sense. > GetProgID.vee was perfect. Cool! It's helped a few people over the years. I did try to do some voice command once but I… Show more
All Activity
Announcement 1 Keysight Discussion Forum Migration to a New Platform!
Announcement:Keysight Discussion Forum Migration to a New Platform!
Hi all, How to bisect a S parameter file by half? I need the resultant S parameter file for de-embedding purpose.
Trending Content
It's that collect, store & simultaneously display thing. You're right, a database certainly would cure the problem. In fact, if the dataset is going to get huge it would be a much better idea. Would also really help crank up efficiency too. Then again, sometimes a minimalist approach is enough of a demo to get the check Plenty of time to worry… Show more
We would like to measure a LNA with frequency range 25GHz to 28GHz and would like to use Downconverter Mode on our N8973A noise figure analyzer. Could you recommend a Downconverter for this application? Does Keysight sell this Downconverter for this application? Does Block downconverters that are used with N8975A will work with N8973A? … Show more
Matters Most
I am connecting to an N9020B via the USB interface and running a Python script that does screen captures to a USB drive using the MMEM:STOR:SCR <filename> command. As far as I can tell, there is no way to copy the screen captures back to the PC via USB interface but I would like to verify that the file was created correctly. For instance, if the… Show more

freedom app Thanks for this great share!
Matters Most
lhornburg, thanks for sharing some sample code and offer your support. I try to capture the DC voltage measurement (max 2.3VDC) with up to 6 decimal place accuracy and plot it over a period of time to evaluate its stability. Below is the code I have been working on to capture 80 measurements of a VDC, max 2.3V, resolution of 10uV. Problems… Show more
Matters Most
I have a USBTMC device prototype In VB.net (with VISA-COM 5.0 library reference), I can open a session using: Dim manager as New Ivi.Visa.Interop.ResourceManager Dim session as Ivi.Visa.IMessage = manager.Open(<valid resource name>) I wanted to get a list of available USB resources using FindRsrc method (manager.FindRsrc("USB0::?*")). I was… Show more
Trending Places
Recommended Content