AnsweredAssumed Answered

BanchVue slow to load DAQ

Question asked by mirek on Jul 27, 2020
Latest reply on Jul 29, 2020 by w0dz

Hello 

Why it taking so long to load each DAQ to BanchVue.

I am using 5 DAQ and each of them required between 2 to 3 minutes to be loaded. What holding this program?

I do not think the PC is nigh be an issue. 

I am running  BanchVue 2019 on 64 bit Window 10 PC with Core I5 and 16 GB memory an solid state HD.

 

Any body have an idea why the loading of hardware in  BanchVue is so slow and if there is a way to improve the speed?

 

Regards.

mirek

 

Outcomes