AnsweredAssumed Answered

Dynamic Mode with two M8190A AWGs

Question asked by maxkeller2312 on May 22, 2020

Hello, 

 

at the moment I'm working with two AWG: M8190A from Keysight and each has two channels. I want to use them in dynamic Mode and one of them as a Primary and the other one as a Secondary. In general I just want to have two sequences and switch between them dynamically. 

 

I'm just able to address the Primary AWG through the dynamic in Port. 

 

Here is my questions: 

         How can I choose which Channel is addressed through the dynamic in Port (1 or 2)

         How can I Start a Sequences which needs both AWGs and all Channels though the dynamic control of just one                               Channel of my Primary AWG ? 

 

Thanks for the help in advance 

Outcomes