AnsweredAssumed Answered

Agilent835x.dll not performing correct command to PNA-X

Question asked by JimmyTE on Feb 13, 2019
Latest reply on Feb 22, 2019 by johanericsson

Hi,

 

I have recently upgraded our PC to Windows 7 and have found that a previous COM programming is not performing the correct function as it did in the past. I ma experiencing this on 5242B,5242A PNA-Xs with Windows XP / Windows 7 OSes.

 

Using the Agilent835x library, the following code

 

"fixture.set_PortMatchingCktModel(1, AgilentPNA835x.NAFixturingPortMatchCkt.naFixPMC_USER)"

 

Does not set port 1 (or 2 if I change that to a 2) to use a user defined S2P file. It actually sets it to use circuit model.

 

Has anyone else ran into this?

Outcomes