AnsweredAssumed Answered

Procedure to perform ZERO/CAL with the 11708A reference attenuator?

Question asked by DBD on Feb 5, 2019
Latest reply on Feb 7, 2019 by Tardz

Hello,

 

 

how do I have to process the real attenuation of my 11708A reference attenuator with 29.86dB (nominal 30dB), when I perform the ZERO/CAL routine of the power meter?

 

I can use the CHANNEL Offset and set it to a value of .14dB. After performing the ZERO/CAL procedure, do I have to clear this generally offset for the measurements?

Do I have to clear the offset for measurements outside of 50MHz?

 

 

Thanks and regards

Robert

Outcomes