AnsweredAssumed Answered

4263B LCR and 16451B Dielectric Test Fixture

Question asked by YoonPham on Jul 11, 2018
Latest reply on Jul 26, 2018 by dk001

Hi guys

I am having some problem with operating the 4263B LCR 100 Hz to 100 kHz when I connect it with 16451B dielectric test fixture. I can't pass the calibration by following the manual. Plus, it is my first time for using 4263B LCR and 16451B dielectric test fixture. Can anyone help with guiding or any procedure for operating them ? How can I calculate the dielectric constant when I obtain the capacitance value ?

 

Thanks 

Outcomes