AnsweredAssumed Answered

82350c with 5890

Question asked by roxletst on May 9, 2017
Latest reply on Oct 3, 2017 by roxletst

Hello, I post this here because I couldn't find the appropiate section in the forum. 

Anyone has any experience connecting a 5890 GC using a 82350C card? I'm using IO Libraries v.15 in a XP machine, but I can't assign the correct Bus Address -it should be 30, but I can only assign up to 29. The other settings are just the same I would set on an older card. Also, I can see the instrument connected in the software with its correct GPIB Address, but when I start Chemstation A.10.02 the GC isn't recognized. 

Any pointer or help would be greatly appreciated,

Thanks

Roxana

Outcomes