AnsweredAssumed Answered

N9038A MXE EMI Receiver - Conducted / Radiated Emissions

Question asked by Zack on Jul 27, 2016
Latest reply on Nov 14, 2017 by bchen94

1) For conducted emissions, should the EMI mode be always set to DC coupling? We noticed when set to AC there would be a high noise floor on the frequencies below 1 MHz.

2) For radiated emissions, Should we keep the EMI mode at AC coupling?

3) It's constantly asking us to keep the receiver aligned. Is this normal? It takes 5-10min to do the full alignment.