AnsweredAssumed Answered

ADS FEM with Momentum Difference in High Frequency High Er

Question asked by hrmoazzen on Jun 25, 2016
Latest reply on Sep 25, 2017 by WDING

Hi

 

I'm working with a high Er (Er=36), 10 mil substrate which I have defined dielectric vias for it and so I must use FEM. When I use the linecalc to calculate for example the width of the microstrip line for Z0=15 ohm, the answer is 26.3 mils. I draw a 100 mils length and 26.3 mils width line in layout and simulate it using FEM and Momentum simulators from 1 GHz to 20 GHz. The return loss of the FEM results is not better than -25 dB for Freq>10 GHz but the results of Momentum analysis seems correct. I have checked this simulation using CST frequency solver and I saw that results are similar to ADS Momentum but differs from ADS FEM.

I tried to change FEM EM setup to get better results which are similar to ADS Momentum and CST but nothing happens.

I should say ADS FEM results for high Er material in high frequency seems to be incorrect. What can I do with this problem?

 

Thanks

Attachments

Outcomes