AnsweredAssumed Answered

transmitted signal coherence on Agilent ENA E5071B

Question asked by Ruthellen on Aug 3, 2010
We have 4-port ENA E5071B in our lab. The setup parameters are: linear sweep, start-frequency=end frequency, continuous trigger.

My understanding is that each CW signal is transmitted after each trigger is fired.  My question is that if the transmitter CW signal is phase coherent. In other words, does the transmitted signal is controlled so that it starts with the same amplitude and phase?

Thank you for the help.