Skip navigation

News

Top & Trending
RadoslavBorisov
Hi, I'm trying to set the GPIB interface to be accessible over the LAN using Agilent IO 14.2 on PNA-L N5240A. It has 2 GPIB82350B cards which work on same IRQ address 11 and the operation system is Windows XP. I'm not able to change the IRQ on one of the cards and I'm not sure if this is really issue. Agilent IO detects only GPIB0
7

Gaëtan
Hello,   I am using TestStand 4.2 to remotely communicate with and control an MXA N9020A to perform bandwidth analysis at -3dBc and lower.  The commands I am using are as per the manual including ":CALC:BWID:NDB-3.00" and ":CALC:BWID:RES?".  All works fine and provides the delta frequency bandwidth at -3dBc.  What I cannot
5
Top & Trending
_new_here_
Hello guys!  I am new to ADS and EM simulations in general, so sorry if I ask some stupid questions.  I am trying to design a PCB with ~5 cm lines which run from 1 surface SMA to another. Simple point to point connection.  I designed the layout of 1 line in Circuit Maker and exported it as ODB data base to ADS. So far
0
Top & Trending
melk
The measurements were on an MF antenna system on which there were signals from local high power AM stations with an amplitude similar to the signal level from the Fieldfox at the input to the antenna matching unit.The matching unit has automatic tuning and resistance adjustment with the objective of providing 50 +j0 ohms at the input. The fieldfox
1