Skip navigation

News

Top & Trending
HSLEE
EMPro Workshop provides various Lab examples to show the complete Electro-Magnetic (EM) simulation flow and the procedure from processes like solid modeling, simulation setup, simulations, data display, and post processing. These lab examples are based on FEM (Finite Element Method) and Finite Difference Time Domain (FDTD) simulation technologies.
0

KeysightOsciloscopes
By Taku Furuta   “I am using a 100 MHz oscilloscope with an included 100 MHz passive probe, I am supposed to be able to measure a 90 MHz sine wave, right?  Is the scope or probe broken?” I hear this sort of question popping up from time to time, understandably since most oscilloscope datasheets do not discuss the
0
Top & Trending
BOB808
I have an MSOX-4054A scope with firmware V04.08.2016071800.  For the life of me I can't get the setup/hold trigger to work.  I can set the setup time to up to <10 seconds but the max allowable hold time is stuck at <10nS.  The scope is hooked up to a relatively slow serial bus with expected setup/hold times in the uS
0